FB#.POLES

Description

FB#.POLES sets the number of individual poles in a resolver feedback device. This variable is used for the commutation function, as well as for velocity feedback scaling, and represents the number of individual poles (not pole pairs). The division value of motor poles (AXIS#.MOTOR.POLES ) and feedback poles (FB#.POLES) must be an integer when moving drive to enable, otherwise a fault is issued.

Context

See Feedback # View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

2 to 510

Default Value

2

Data Type

Integer

See Also

AXIS#.MOTOR.POLES
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
FB1.POLES

3500h

03h

Unsigned16

-

-

Read/Write

No

FB2.POLES

3501h

03h

Unsigned16

-

-

Read/Write

No

FB3.POLES

3502h

03h

Unsigned16

-

-

Read/Write

No

FB4.POLES

3503h

03h

Unsigned16

-

-

Read/Write

No

FB5.POLES

3504h

03h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

FB1.POLES

30100

7594

Unsigned16

Read/Write

-

FB2.POLES

30101

7595

Unsigned16

Read/Write

-

FB3.POLES

30102

7596

Unsigned16

Read/Write

-

FB4.POLES

30103

7597

Unsigned16

Read/Write

-

FB5.POLES

30104

7598

Unsigned16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.POLES

30100

Unsigned16

Read/Write

-

FB2.POLES

30101

Unsigned16

Read/Write

-

FB3.POLES

30102

Unsigned16

Read/Write

-

FB4.POLES

30103

Unsigned16

Read/Write

-

FB5.POLES

30104

Unsigned16

Read/Write

-